Is there a reason SDCKE 0 is paired with CLK1 rather than CLK0?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there a reason SDCKE 0 is paired with CLK1 rather than CLK0?

Jump to solution
928 Views
katrinagundal-z
Contributor I

Looking at the multiple reference designs including the sabre board (dual-lite), the DRAM appears to be using the CLK1 clock pair with SDCKE0. Is there a reason SDCKE 0 is paired with CLK1 rather than CLK0?

We were unable to find an explanation in the chip documentation so if you could provide further info it would be greatly appreciated. We are trying to close out a design review...

Labels (6)
0 Kudos
1 Solution
743 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

View solution in original post

0 Kudos
3 Replies
744 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 Kudos
743 Views
Yuri
NXP Employee
NXP Employee

The SDRAM clock signals are the same, assuming that the clock delays are the same.

Please look at section 44.12.53 [MMDC PHY CK Control Register (MMDCx_MPSDCTRL)]

of the Reference Manual [IMX6DQRM(Rev.2)] and section 17 (Clock Delay Calibration) of the

app note AN4467 about registers MMDC1_MPSDCTRL and MMDC2_MPSDCTRL, which are named

as SDCTRL[SDCLK0_DEL] and SDCTRL[SDCLK1_DEL] in the app note.

Regards,

Yuri.

0 Kudos
743 Views
igorpadykov
NXP Employee
NXP Employee

Hi Katrina

CLK1 and CLK0 clock are the same signals, so

no difference which to use.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos