Is there a patch to improve spi nor read speed in Uboot

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is there a patch to improve spi nor read speed in Uboot

1,123件の閲覧回数
ivyliu
Contributor IV

Hi All,

Spi nor can work with DMA in Linux.

Is there a patch to make spi nor work with DMA in Uboot too?

I am using Imx6Solo.

Thanks and Best Regards,

Ivy

0 件の賞賛
返信
2 返答(返信)

979件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

HI Ivy

please look at

Linux Fast Boot on i.MX6 Sabresd Board

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

979件の閲覧回数
ivyliu
Contributor IV

Hi Igor,

Thank you very much for your reply.

I checked that one before.

The patch is for MMC+DMA, not spi nor.

Best Regards,

Ivy

0 件の賞賛
返信