Is there a patch to improve spi nor read speed in Uboot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there a patch to improve spi nor read speed in Uboot

1,145 Views
ivyliu
Contributor IV

Hi All,

Spi nor can work with DMA in Linux.

Is there a patch to make spi nor work with DMA in Uboot too?

I am using Imx6Solo.

Thanks and Best Regards,

Ivy

0 Kudos
Reply
2 Replies

1,001 Views
igorpadykov
NXP Employee
NXP Employee

HI Ivy

please look at

Linux Fast Boot on i.MX6 Sabresd Board

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,001 Views
ivyliu
Contributor IV

Hi Igor,

Thank you very much for your reply.

I checked that one before.

The patch is for MMC+DMA, not spi nor.

Best Regards,

Ivy

0 Kudos
Reply