Is there a flag in the I.MX6 that signals when an EEPROM Recovery boot is performed?

cancel
Showing results for 
Search instead for 
Did you mean: 

Is there a flag in the I.MX6 that signals when an EEPROM Recovery boot is performed?

150 Views
andrelabelle
Contributor I

Hi,

I have my fuses programmed to boot from SD and I also have the EEPROM Recovery bit set.

U-Boot is on both the SD card and the SPI-NOR flash.

Normally the system boots from the SD. If I wipe U-Boot from the SD the system boots from SPI-NOR.

So my question is: Once the I.MX6 is booted from SPI-NOR, is there any way for it to detect that it has booted from SPI-NOR and not the SD card?

Thanks,

Andre

Labels (1)
Tags (2)
0 Kudos
1 Reply

54 Views
igorpadykov
NXP TechSupport
NXP TechSupport

Hi andre

there is no such flag for recovery.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos