Is there a demo about 1-wire uart in the rt595 SDK?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there a demo about 1-wire uart in the rt595 SDK?

1,074 Views
Dave_SU
Contributor III

Hi,

My HW, TX and RX are connected together, with a 1K resistor in the middle. Then connect to the UART debug board (the debug board can enumerate a UART port for communication, and has single-line and dual-line UART conversion function).

My assumption is that when use TX,  disable RX, and when use RX, disable TX. But I don't know how to disable TX or RX.

MCU: RT595

Tags (1)
0 Kudos
Reply
2 Replies

1,055 Views
Dave_SU
Contributor III

@Omar_Anguiano 

thanks, let me try it.

0 Kudos
Reply

1,067 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello
Hope you are well.
Unfortunately, we don´t have an example using 1-wire UART.
I apologize for the inconvenience this may cause you.
To disable RX and TX you need to disable the corresponding FIFO in FIFOCFG register.

If you have more questions do not hesitate to ask me.
Best regards,
Omar

0 Kudos
Reply