Is there a PAL/NTSC Video Decoder Supported by iMX8MQ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there a PAL/NTSC Video Decoder Supported by iMX8MQ?

1,000 Views
leandroschmitz
Contributor I

Hello, 

I need to interface a PAL/NTSC Camera with my custom board using iMX8MQ, I try to use ISL79987 with no success.

I'd like to know If there is a Solution with driver compatible with iMX8MQ, ie, just one channel, a format compatible with gst-launch-1.0, and no need of 2D GPU.

Thank you.

0 Kudos
1 Reply

927 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello  Leandro Schmitz,

i.MX8MQ supports 2 MIPI CSI-2 ports, which are camera input interface. so you need to use CVBS to MIPI CSI-2  Bridge for your application, like ADV7280-M. BUT each MIPI CSI-2 of i.MX8MQ can only support 1 channel camera, like this:

(1) MIPI CSI1: 1 camera with PAL/NTSC--->ADV7280-M--->MIPI CSI1

(2) MIPI CSI2: 1 camera with PAL/NTSC--->ADV7280-M--->MIPI CSI2

Hope the information is helpful to you!

Have a nice day!

B.R,

Weidong

0 Kudos