Is there Android BSP for IMX6 SOLO SABRE SD board?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there Android BSP for IMX6 SOLO SABRE SD board?

900 Views
sreeharshap
Contributor II

Hello there, 

Is there Android BSP for IMX6 SOLO SABRE SD?

I can see YOCTO is available for IMX6 SOLO SABRE SD but I'm unable to find ANDROID BSP. 

Thanks

Labels (1)
0 Kudos
Reply
3 Replies

722 Views
art
NXP Employee
NXP Employee

1. There is no i.MX6Solo SABRE SD board. Only the i.MX6Quad and i.MX6DualLite SABRE SD boards are available from NXP.

2. The current M6.0.1_2.1.0 i.MX6 Android BSP allows to build the target images for all i.MX6 family processors, including the i.MX6Solo. The source code BSP and pre-built demo images for various processors/boards are available here:

http://www.nxp.com/products/software-and-tools/software-development-tools/i.mx-software-and-tools/an...

The related documentation is available here:

http://www.nxp.com/products/software-and-tools/software-development-tools/i.mx-software-and-tools/an...


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

722 Views
sreeharshap
Contributor II

Hi Artur

Thanks so much for your prompt update and suggestions.

It was very helpful.

Warm regards

Pole

0 Kudos
Reply

722 Views
joanxie
NXP TechSupport
NXP TechSupport

one can find android source code and demo image from the link as below:

<Android OS for i.MX Applications Processors|NXP >.

0 Kudos
Reply