Is the pin/pad CSI0_DATA_EN (iMX 6 Quad Core) only option to output ARM clock?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is the pin/pad CSI0_DATA_EN (iMX 6 Quad Core) only option to output ARM clock?

533 Views
manojprabahar
Contributor I

Is the pin/pad CSI0_DATA_EN only option to output ARM clock off from processor, to ensure that the core is operating at configured speed? Even if so, whether the GPIO is capable to do so? Because when we tried to output the clock via GPIO earlier, it didnt go beyond 400MHz!

Labels (2)
Tags (2)
0 Kudos
1 Reply

454 Views
igorpadykov
NXP Employee
NXP Employee

Hi Manoj

please consider signals CCM_CLKO1, 2 with register CCM_CCOSR (output arm_clk_root)

described in sect.18.6.21 CCM Clock Output Source Register (CCM_CCOSR)

i.MX6DQ Reference Manual

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos