Is some spec of MMPF0100 buck regulator changed when changed SWx_PWRSTG[2:0]?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is some spec of MMPF0100 buck regulator changed when changed SWx_PWRSTG[2:0]?

ソリューションへジャンプ
1,886件の閲覧回数
satoshishimoda
Senior Contributor I

Hi community,

Our customer have a question about MMPF0100.

Please see chapter 6.4.4.2.3 in MMPF0100 datasheet.

They want to know whether some specification of buck regulator is changed when change the current configuration SWx_PWRSTG[2:0].

For example, set SW2_PWRSTG[2:0] from 2.0A to 0.75A when the load current is 200mA.

In this case, is some specification (efficiency, duty, etc...) change?

Best Regards,

Satoshi Shimoda

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,618件の閲覧回数
art
NXP Employee
NXP Employee

The setting of the SWx_PWRSTG[2:0] bits just change the number of FETs working in parallel to drive the inductor. In the case you describe (SW2 is set for 0.75A max. load whereas the actual load current is 200mA) no changes in efficiency or other SW2 parameters will occur.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,619件の閲覧回数
art
NXP Employee
NXP Employee

The setting of the SWx_PWRSTG[2:0] bits just change the number of FETs working in parallel to drive the inductor. In the case you describe (SW2 is set for 0.75A max. load whereas the actual load current is 200mA) no changes in efficiency or other SW2 parameters will occur.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信