Is qnx bsp available for i.MX8?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is qnx bsp available for i.MX8?

4,343 Views
yangwei
Contributor I

Hello All,

We have MCIMX8QXP-CPU and MCIMX8M-EVK boards on hands.

May I know if qnx bsp packages available for them?

0 Kudos
9 Replies

3,677 Views
dantx
Contributor I

One option is QNX BSP provided by Blackberry for the Toradex Apalis i.MX8 QuadMax SoM

https://www.toradex.com/operating-systems/qnx

 

Getting Started: https://developer.toradex.com/knowledge-base/partner-demo-image-qnx-neutrino-real-time-operating-sys...

 

0 Kudos

3,773 Views
yangwei
Contributor I

Thanks for your reply.

I hear that i.MX8 has different types e.g: i.MX 8QuadMax A0, i.MX 8QuadXPlus A0, i.MX 8M Quad,i.MX 8M Mini, i.MX 8QuadXPlus B0 and i.MX 8QuadMax B0
May I know what the differences are between them?

0 Kudos

3,773 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Wei Yang,

For details on the different iterations of the i.MX8M you can refer to the i.MX8M Fact Sheet (link below)

https://www.nxp.com/docs/en/fact-sheet/i.MX8M-FS.pdf

For the i.MX8MM please refer to the following Fact Sheet:

https://www.nxp.com/docs/en/fact-sheet/IMX8MMINIFS.pdf

As for the i.MX8QuadMax and i.MX8QuadX variants, I would need to ask you to please contact your FAE as these processors have not been released and there is no public technical information available yet.

My apologies for the inconvenience.

Regards,

0 Kudos

3,773 Views
vfilip
NXP Employee
NXP Employee

Hi,

BSP for MCIMX8QXP-CPU and MCIMX8M-EVK (Engineering release only) boards are available. In case these BSP are not in QNX software center you might ask QNX for details.

best regards

Vojtech Filip

0 Kudos

3,773 Views
imman
Senior Contributor II

Hello,

iWave has matured QNX BSP for the i.MX8Quadx B0. Product link is here.

https://www.iwavesystems.com/product/cpu-modules/smarc-modules/i-mx-8-board/imx8-quadmax-smarc-som.h... 

It is also listed in the QNX website; Search for i.MX8 here;

QNX Board Support Packages 

iWave also provide QNX porting services to all variations of i.MX8 (i.MX8X, i.MX8M, i.MX8M mini etc).

Thanks, Immanuel

0 Kudos

1,683 Views
paultran
Contributor I
hi imman
we're looking for QNX imx8m mini
please advise more detail
0 Kudos

3,773 Views
yangwei
Contributor I

QNX Software Center does not have the BSP for the MCIMX8QXP-CPU and MCIMX8M-EVK boards.

Is any way to get the bsp for these boards? 

0 Kudos

3,773 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Wei Yang,

Since these are NXP board there is not a QNX available for these. You may contact NXP Professional Services and ask if it would be possible to port QNX for them.

My apologies for the inconvenience.

Regards,

0 Kudos

3,773 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Wei Yang,

We do not provide a QNX BSP, but some third parties do provide QNX BSPs for their boards.

http://blackberry.qnx.com/en/support/qnx-board-support-packages

If you need further help, please contact your sales or FAE and they may be able to provide some more guidance.

Regards,

0 Kudos