Is ltp-imx for linux supported for iMX.6D? I read elsewhere that iMX.6Q does not support it? If it is not supported, are there any alternatives to validate kernel, sys calls in linux?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is ltp-imx for linux supported for iMX.6D? I read elsewhere that iMX.6Q does not support it? If it is not supported, are there any alternatives to validate kernel, sys calls in linux?

909 Views
kathiravanraviv
Contributor I

I am working on a custom board based on iMX6D. Yocto Linux has been used in this board and I am analyzing if ltp packages can be integrated. It is mentioned that iMX6.Q does not support ltp. Does iMX6.D support it? If not, are there any alternatives that can be used?

Labels (2)
0 Kudos
Reply
1 Reply

831 Views
joanxie
NXP TechSupport
NXP TechSupport

 I got reply as below:

"

Unfortunately ltp-imx package is not supported by Freescale for i.MX6 platform.

Sorry for the inconvenience.

The package ltp-imx was used for early i.MX series, such as i.MX35,51.

Then it was replaced with OBDS - i.MX50,53,28.

"

for mx6, one can use SDK which includes OBDS.

0 Kudos
Reply