Is it possible to work with SD Card and WIFI/BLUETOOTH at the same time on mimxrt1170-evk?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is it possible to work with SD Card and WIFI/BLUETOOTH at the same time on mimxrt1170-evk?

Jump to solution
673 Views
SCh
Contributor II

Hi, it looks like SD Card and WIFI\BLUETOOTH working on the same sd-interface. Is that possible to run them both at the same time?

Labels (1)
0 Kudos
Reply
1 Solution
657 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @SCh ,

  Thank you for your interest in the NXP MIMXRT product, I would like to provide service for you.

  About the SD card and the WIFI/BLUETHOOTH module work at the same time, you just need to check, whether the MIMXRT1170-EVK these two modules share the same interface or not.

  Please check the schematic:

 

kerryzhou_0-1693197797969.png

kerryzhou_1-1693197806106.png

 

kerryzhou_2-1693197814176.png

 

 

You can see, to the SDHC interface, the sdcard and the WIFI/Bluethooth share the same interface, so in the MIMXRT1170-EVK, you can't work at the same time for the same SDHC interface.

But, if the wifi/bluethooth don't use the SDHC interface for the communication, then you can use both of them.

 

Wish it helps you!

Best Regards,

Kerry

 

 

View solution in original post

0 Kudos
Reply
1 Reply
658 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @SCh ,

  Thank you for your interest in the NXP MIMXRT product, I would like to provide service for you.

  About the SD card and the WIFI/BLUETHOOTH module work at the same time, you just need to check, whether the MIMXRT1170-EVK these two modules share the same interface or not.

  Please check the schematic:

 

kerryzhou_0-1693197797969.png

kerryzhou_1-1693197806106.png

 

kerryzhou_2-1693197814176.png

 

 

You can see, to the SDHC interface, the sdcard and the WIFI/Bluethooth share the same interface, so in the MIMXRT1170-EVK, you can't work at the same time for the same SDHC interface.

But, if the wifi/bluethooth don't use the SDHC interface for the communication, then you can use both of them.

 

Wish it helps you!

Best Regards,

Kerry

 

 

0 Kudos
Reply