Is it possible to use the MCIMX23LCD LCD display from the i.MX23-EVK into the i.MX28-EVK board?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Is it possible to use the MCIMX23LCD LCD display from the i.MX23-EVK into the i.MX28-EVK board?

跳至解决方案
1,614 次查看
ismaelinfante
Contributor I

Hi,

I want to use the MCIMX23LCD LCD display from the i.MX23-EVK board into the i.MX28-EVK board.

I noticed that the display driver for this LCD is present into the BSP of the i.MX28-EVK (BSP_10_08_02), located at
PLATFORM\iMX28-EVK-PDK1_9\SRC\DRIVERS\DISPLAY\lms430.cpp.

What is the procedure to build an NK.bin that makes use of this driver instead of the PLATFORM\iMX28-EVK-PDK1_9\SRC\DRIVERS\DISPLAY\43wvf1g.cpp driver?

Is it necessary to do some changes into the EBOOT also in order to support this LCD display?

Thanks in advance,

Ismael Infante

标签 (1)
标记 (4)
0 项奖励
回复
1 解答
1,385 次查看
JorgeRama_rezRi
NXP Employee
NXP Employee

Hi Ismael,

Both LCD connectors have almost the same pin-out, unfortunately, there are a few differences that will make the systems not fully compatible, plus, the MX23 LCD is a WQVGA, and the MX28 LCD is a WVGA, so this may result in the need for SW changes too. So the answer is: You can't just connect the MX23 LCD into the MX28 without a few changes in HW and SW. You can check the differences between the connectors in the schematics found in the web page. I'm not a SW guy but I guess looking at the driver in the BSP can tell you what you need in that area too.

Best regards.

Jorge.

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,386 次查看
JorgeRama_rezRi
NXP Employee
NXP Employee

Hi Ismael,

Both LCD connectors have almost the same pin-out, unfortunately, there are a few differences that will make the systems not fully compatible, plus, the MX23 LCD is a WQVGA, and the MX28 LCD is a WVGA, so this may result in the need for SW changes too. So the answer is: You can't just connect the MX23 LCD into the MX28 without a few changes in HW and SW. You can check the differences between the connectors in the schematics found in the web page. I'm not a SW guy but I guess looking at the driver in the BSP can tell you what you need in that area too.

Best regards.

Jorge.

0 项奖励
回复