Is it possible to use the MCIMX23LCD LCD display from the i.MX23-EVK into the i.MX28-EVK board?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is it possible to use the MCIMX23LCD LCD display from the i.MX23-EVK into the i.MX28-EVK board?

ソリューションへジャンプ
1,618件の閲覧回数
ismaelinfante
Contributor I

Hi,

I want to use the MCIMX23LCD LCD display from the i.MX23-EVK board into the i.MX28-EVK board.

I noticed that the display driver for this LCD is present into the BSP of the i.MX28-EVK (BSP_10_08_02), located at
PLATFORM\iMX28-EVK-PDK1_9\SRC\DRIVERS\DISPLAY\lms430.cpp.

What is the procedure to build an NK.bin that makes use of this driver instead of the PLATFORM\iMX28-EVK-PDK1_9\SRC\DRIVERS\DISPLAY\43wvf1g.cpp driver?

Is it necessary to do some changes into the EBOOT also in order to support this LCD display?

Thanks in advance,

Ismael Infante

ラベル(1)
タグ(4)
0 件の賞賛
返信
1 解決策
1,389件の閲覧回数
JorgeRama_rezRi
NXP Employee
NXP Employee

Hi Ismael,

Both LCD connectors have almost the same pin-out, unfortunately, there are a few differences that will make the systems not fully compatible, plus, the MX23 LCD is a WQVGA, and the MX28 LCD is a WVGA, so this may result in the need for SW changes too. So the answer is: You can't just connect the MX23 LCD into the MX28 without a few changes in HW and SW. You can check the differences between the connectors in the schematics found in the web page. I'm not a SW guy but I guess looking at the driver in the BSP can tell you what you need in that area too.

Best regards.

Jorge.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,390件の閲覧回数
JorgeRama_rezRi
NXP Employee
NXP Employee

Hi Ismael,

Both LCD connectors have almost the same pin-out, unfortunately, there are a few differences that will make the systems not fully compatible, plus, the MX23 LCD is a WQVGA, and the MX28 LCD is a WVGA, so this may result in the need for SW changes too. So the answer is: You can't just connect the MX23 LCD into the MX28 without a few changes in HW and SW. You can check the differences between the connectors in the schematics found in the web page. I'm not a SW guy but I guess looking at the driver in the BSP can tell you what you need in that area too.

Best regards.

Jorge.

0 件の賞賛
返信