Is it possible to use mxc_poll as blocking operation ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is it possible to use mxc_poll as blocking operation ?

1,263件の閲覧回数
alexisfronteau
Contributor III

Hi, 

I'm trying to use poll in mxc_v4l2_capture as blocking and it wakes up only when a frame arrived or if a timeout occured.

But it seems impossible to do, poll function never wait for image. So I would like to know if it is an error or if i've missed something

Thanks

ラベル(3)
0 件の賞賛
返信
2 返答(返信)

1,168件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Alexis

Here are some app that can help:

https://community.nxp.com/message/887973

0 件の賞賛
返信

1,168件の閲覧回数
alexisfronteau
Contributor III

Hi, 

Thanks for your reply. I have already read this post, so the only way is to patch the mxc_v4l2_capture driver

0 件の賞賛
返信