Is it possible to have the u-boot on a FAT32 partion?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Is it possible to have the u-boot on a FAT32 partion?

3,021 次查看
mzhang
Contributor I

Hi,

Here the current structure of the SD card we are using to boot the device:

1st partition: u-boot

2nd: boot

3rd: linux (root)

pastedImage_1.png

I'm wondering if it is possible to have something like this (a SD card for raspberry):

pastedImage_2.png

We'd like to be able to put a config file on a FAT32 boot partition which configures the device at boot.

This config file must be editable from a Windows machine.

The thing is Windows only "mount" the first partition of an "usb device", so it only see the 1st u-boot partition. (Windows 10 Creator Update allows to mount all the partitions, but from my test, it's not always working, and it doesn't recognize FAT12.)

Thanks.

MZ

标签 (3)
标记 (3)
0 项奖励
回复
2 回复数

2,558 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Which board are you using?

0 项奖励
回复

2,558 次查看
mzhang
Contributor I

MCIMX283CVM4B

0 项奖励
回复