Is it possible to enable the Deep Sleep Mode in the IMX8M_EVK from under the bootloader?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Is it possible to enable the Deep Sleep Mode in the IMX8M_EVK from under the bootloader?

1,328 次查看
sergeyan
Contributor II

Hi!

Is it possible to enable the Deep Sleep Mode in the IMX8M_EVK from under the bootloader, using the commands mw\md in accordance with the reference manual for IMX8M?

I am using Example 3 (page 676 of i.MX 8M Dual/8M QuadLite/8M Quad Applications Processors Reference Manual Rev.3).

By the way, there are typos in the examples (wrong addresses)..

Thank you!

0 项奖励
回复
2 回复数

1,311 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Sergey

 

ussually bootloaders do not support interrupts, so seems not possible to wake processor.

For examples one can look at sect.2.5 Power Management   i.MX Linux Reference Manual​

 

Best regards
igor

0 项奖励
回复

1,300 次查看
sergeyan
Contributor II

Hi Igor

My task is to estimate the minimum CPU heat dissipation while keeping Linux running (1 core, minimum frequency, minimum interfaces). For reference - work in the bootloader (without Linux) - 45 degrees with a radiator.

I tried to reproduce example 3 with the mw commands, but did not get any response - either the example is designed to be used from under Linux, or there are errors in the example.

Best regards
Sergey

 

0 项奖励
回复