Is it possible to enable iMX6UL's EPIT in STOP mode?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is it possible to enable iMX6UL's EPIT in STOP mode?

ソリューションへジャンプ
1,529件の閲覧回数
kevinroussel
Contributor II

Hello,

I am optimizing the power consumption of an embedded device based on the iMX6UL processor. My aim is to leave it sleeping as long as possible, using the EPIT to wake it up regularly as needed.

Currently, I am able (thanks to a custom Linux kernel module) to use EPIT interrupts to wake up my system from WAIT mode. But power consumption in WAIT mode is still quite high for my purposes.

Thus, is there a wait to keep EPIT enable in STOP mode on the iMX6UL?

(According to the processor manual (CCM chapter), programming the CCGR1 register allows to keep EPIT clocks running only in run and WAIT mode. Similarly, setting the MOD_EN_OV_EPIT bit in CMEOR register doesn't seem to have any effect.)

Thanks in advance for any comment or advice,

ラベル(2)
タグ(3)
0 件の賞賛
返信
1 解決策
1,449件の閲覧回数
kevinroussel
Contributor II

Hello Igor,

Thanks for your answer. I forgot to state that I did set the STOPEN bit in the EPITx_CR register.

In the meantime, I found the answer to my problem: I configured the EPIT with the standard peripheral clock (putting 1 in CLKSRC field of EPITx_CR register), while this clock is disabled in STOP mode. I thus switched to the reference low-frequency clock (putting 3 in CLKSRC field of EPITx_CR register); this solved my problem, I can now use EPIT to wake up my system from STOP mode after a given delay.

Best regards,

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,449件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Kévin

one can check bit STOPEN in register EPITx_CR and description in

sect.23.4.3.2 Low-Power Mode Behavior i.MX6UL Reference Manual

http://www.nxp.com/docs/en/reference-manual/IMX6ULRM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,450件の閲覧回数
kevinroussel
Contributor II

Hello Igor,

Thanks for your answer. I forgot to state that I did set the STOPEN bit in the EPITx_CR register.

In the meantime, I found the answer to my problem: I configured the EPIT with the standard peripheral clock (putting 1 in CLKSRC field of EPITx_CR register), while this clock is disabled in STOP mode. I thus switched to the reference low-frequency clock (putting 3 in CLKSRC field of EPITx_CR register); this solved my problem, I can now use EPIT to wake up my system from STOP mode after a given delay.

Best regards,

0 件の賞賛
返信