Is it possible to debug i.mx8x with gdb debugger running on windows host?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is it possible to debug i.mx8x with gdb debugger running on windows host?

1,307件の閲覧回数
anaseem
Contributor IV

MCIM X8QXP-CPU evaluation board is running embedded Linux.  Is it possible to debug with gdb debugger running on windows host?

ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,199件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Amer

one can check below link which may be helpful

How to JTAG debug iMX8mq? 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,199件の閲覧回数
anaseem
Contributor IV

Or can embedded Linux target be debugged from gdb debugger running from terminal that is connected to Linux Server?

0 件の賞賛
返信