Is it possible to connect camera with CameraLink to imx53 CSI??

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Is it possible to connect camera with CameraLink to imx53 CSI??

跳至解决方案
1,982 次查看
bamboosso
Contributor II

Hello,

Is it possible to connect camera with CameraLink to imx53 CSI??

Some kind of converter (single chip would be nice) should do the job, but I can't find one.

Does anyone already done it?? Any kind of experience appreciated.

Regards,

Maciek

标签 (3)
标记 (2)
0 项奖励
回复
1 解答
1,404 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Maciej

if CameraLink waveforms are compatible with

i.MX53 CI, then yes. CSI waveforms are given in

sect.4.7.7.2 Sensor Interface Timings

i.MX53 Datasheet (rev.6, 3/2013)

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX53CEC.pdf

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,405 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Maciej

if CameraLink waveforms are compatible with

i.MX53 CI, then yes. CSI waveforms are given in

sect.4.7.7.2 Sensor Interface Timings

i.MX53 Datasheet (rev.6, 3/2013)

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX53CEC.pdf

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复