Is it possible to connect camera with CameraLink to imx53 CSI??

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is it possible to connect camera with CameraLink to imx53 CSI??

Jump to solution
1,919 Views
bamboosso
Contributor II

Hello,

Is it possible to connect camera with CameraLink to imx53 CSI??

Some kind of converter (single chip would be nice) should do the job, but I can't find one.

Does anyone already done it?? Any kind of experience appreciated.

Regards,

Maciek

Labels (3)
Tags (2)
0 Kudos
Reply
1 Solution
1,341 Views
igorpadykov
NXP Employee
NXP Employee

Hi Maciej

if CameraLink waveforms are compatible with

i.MX53 CI, then yes. CSI waveforms are given in

sect.4.7.7.2 Sensor Interface Timings

i.MX53 Datasheet (rev.6, 3/2013)

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX53CEC.pdf

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,342 Views
igorpadykov
NXP Employee
NXP Employee

Hi Maciej

if CameraLink waveforms are compatible with

i.MX53 CI, then yes. CSI waveforms are given in

sect.4.7.7.2 Sensor Interface Timings

i.MX53 Datasheet (rev.6, 3/2013)

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX53CEC.pdf

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply