Is it possible to configure Slew Rate of HDMI or LVDS pins on i.MX6DL?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is it possible to configure Slew Rate of HDMI or LVDS pins on i.MX6DL?

Jump to solution
1,974 Views
andrejakostic
Contributor II

I'd just like to confirm if the slew rate and drive strength are configurable for the LVDS (LVDS0 CLK p/n and Data 0/1/2 p/n) and HDMI(TX CLK p/n and TX Data 0/1/2 p/n) pins on the i.MX6DL.


As far as I can understand from reading the reference manual, the LVDS pins have fixed configuration, which cannot be changed in the software, and the slew rate of the HDMI pins cannot be configured in software, but the drive strength is configurable using the procedure explained in the chapter 35.8 of the reference manual.

So is the above correct?

Labels (1)
1 Solution
1,857 Views
igorpadykov
NXP Employee
NXP Employee

Hi Andreja

I think this is correct understanding.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
1,858 Views
igorpadykov
NXP Employee
NXP Employee

Hi Andreja

I think this is correct understanding.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------