Is it possible to autostart MfgTool 2.3.4 download ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Is it possible to autostart MfgTool 2.3.4 download ?

1,341 次查看
nicolaporzi
Contributor I

Hello,

we are currently using MfgTool 2.3.4 with gui to load a bsp on iMX6.

We are developing an EOL test bench and we need to run MfgTool from a C# environment but we would not have any interaction with the operator at automatic EOL testing bench. Is it possible to set some parameters so when launched the MfgTool automatically download code without pressing "START" button ?

Thanks

0 项奖励
回复
2 回复数

1,154 次查看
nicolaporzi
Contributor I

Hello, thanks.

I launch it with -noui option and it works but the process never stops. I would launch in EOL automatic sequence by c# sw but I can't have any response because the process never ends and it's not giving any return code when programming is done (i.e. 0 success, 1 fail) Is there any other option to use this sw in production environments ?
Thanks,

Nicola 

1,154 次查看
art
NXP Employee
NXP Employee

MFGtool can be started and operated from the command line, refer to the attached document for details.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复