Is it possible to 24 MHz oscillator instead of crystal on i.MX28?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Is it possible to 24 MHz oscillator instead of crystal on i.MX28?

跳至解决方案
1,681 次查看
jschoen
Contributor III

Is it possible to connect a 24 Mhz oscillator to XTALO of i.MX28 instead of using 24 MHz crystal?  I don't see any documentation on bypassing the internal oscillator.

Thanks.

标签 (1)
0 项奖励
回复
1 解答
1,362 次查看
Yuri
NXP Employee
NXP Employee

   Generally, it seems to be possible to apply an external 24MHz clock signal

to XTALI and leave XTALO open, however, the amplitude of an external clock

signal must not exceed VDDXTAL, that is typically around 1.0V.

   Next, an external oscillator may be connected to XTALO pin instead of XTALI pin. In addition,
an AC coupling capacitor should be place close to the i.MX28 so that the internal bias of the
i.MX28 circuit will not be affected.
   However, this configuration is not recommended in practice. The XTALO  as input is a high-impedance

one and therefore it increases noisy environment of the whole i.MX28, including the DCDC converters.

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,363 次查看
Yuri
NXP Employee
NXP Employee

   Generally, it seems to be possible to apply an external 24MHz clock signal

to XTALI and leave XTALO open, however, the amplitude of an external clock

signal must not exceed VDDXTAL, that is typically around 1.0V.

   Next, an external oscillator may be connected to XTALO pin instead of XTALI pin. In addition,
an AC coupling capacitor should be place close to the i.MX28 so that the internal bias of the
i.MX28 circuit will not be affected.
   However, this configuration is not recommended in practice. The XTALO  as input is a high-impedance

one and therefore it increases noisy environment of the whole i.MX28, including the DCDC converters.

0 项奖励
回复