Is it available to use USB as displaying port?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is it available to use USB as displaying port?

1,304件の閲覧回数
yibhan
Contributor III

Hi guys,

I have consideration that is available to display video to USB without converting hardware chip.

I just am considering Imx8x/imx6q chip for this functions. Anyway, I don't want to use converting chip from LVDS to USB.

If it is available, which of chips are available and any more modification for driver?

Thanks

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

1,300件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi yibhan

 

I am afraid i.MX8 does not support such capability, sorry.

 

Best regards
igor

0 件の賞賛
返信

1,285件の閲覧回数
yibhan
Contributor III

Hi guys,

Thank you for answering,

I have an additional question, how about imx6x ?

0 件の賞賛
返信

1,283件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

it is the same.

 

~igor

0 件の賞賛
返信

1,279件の閲覧回数
yibhan
Contributor III

Hi guys,

Thank you for answering,

I have an additional question. Do you have any software patch for my request?

thanks,

0 件の賞賛
返信