Is it available to use USB as displaying port?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is it available to use USB as displaying port?

539 Views
yibhan
Contributor III

Hi guys,

I have consideration that is available to display video to USB without converting hardware chip.

I just am considering Imx8x/imx6q chip for this functions. Anyway, I don't want to use converting chip from LVDS to USB.

If it is available, which of chips are available and any more modification for driver?

Thanks

0 Kudos
4 Replies

535 Views
igorpadykov
NXP Employee
NXP Employee

Hi yibhan

 

I am afraid i.MX8 does not support such capability, sorry.

 

Best regards
igor

0 Kudos

520 Views
yibhan
Contributor III

Hi guys,

Thank you for answering,

I have an additional question, how about imx6x ?

0 Kudos

518 Views
igorpadykov
NXP Employee
NXP Employee

it is the same.

 

~igor

0 Kudos

514 Views
yibhan
Contributor III

Hi guys,

Thank you for answering,

I have an additional question. Do you have any software patch for my request?

thanks,

0 Kudos