Hi,
In older threads, I see references to a baremetal SDK - imx6_platform_sdk_v1.1.0.tgz archive, some SDK with possible additional information about JTAG and mfgtool interfaces.
Could not locate the archive in the link provided for "i.MX 6 series platform SDK" from the following thread.
https://community.freescale.com/thread/313792
Is this SDK obsolete for IMX6UL architecture or still a valid archive? There is another SDK archive "fsl-gpu-sdk-2.3.bin" available though.
Thanks,
Mahesh
Solved! Go to Solution.
Hello,
shortly - "imx6_platform_sdk_v1.1.0" is not valid (supported) and
it was not intended for i.MX6UL.
""fsl-gpu-sdk-2.3.bin" - this is just for GPU of i.MX6.
Regards,
Yuri.
Ok thanks both.
Hi Mahesh,
Our expert has given you reply, please have a check. Here usb otg port is supported, so recommend you to use the mfgtool.
Have a nice day
Dan
Hello,
shortly - "imx6_platform_sdk_v1.1.0" is not valid (supported) and
it was not intended for i.MX6UL.
""fsl-gpu-sdk-2.3.bin" - this is just for GPU of i.MX6.
Regards,
Yuri.