Is imx6_platform_sdk_v1.1.0.tgz archive valid and applicable for IMX6UL?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is imx6_platform_sdk_v1.1.0.tgz archive valid and applicable for IMX6UL?

Jump to solution
2,711 Views
maheshbalasubra
Contributor I

Hi,

In older threads, I see references to a baremetal SDK - imx6_platform_sdk_v1.1.0.tgz archive, some SDK with possible additional information about JTAG and mfgtool interfaces.

Could not locate the archive in the link provided for "i.MX 6 series platform SDK" from the following thread.

https://community.freescale.com/thread/313792

Is this SDK obsolete for IMX6UL architecture or still a valid archive?  There is another SDK archive "fsl-gpu-sdk-2.3.bin" available though.

Thanks,

Mahesh

Labels (1)
0 Kudos
Reply
1 Solution
2,000 Views
Yuri
NXP Employee
NXP Employee

Hello,

  shortly - "imx6_platform_sdk_v1.1.0" is not valid (supported) and

it was not intended for i.MX6UL.
""fsl-gpu-sdk-2.3.bin" - this is just for GPU of i.MX6.

Regards,

Yuri.

View solution in original post

3 Replies
2,000 Views
maheshbalasubra
Contributor I

Ok thanks both.

0 Kudos
Reply
2,000 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Mahesh,

Our expert has given you reply, please have a check. Here usb otg port is supported, so recommend you to use the mfgtool.

Have a nice day

Dan

2,001 Views
Yuri
NXP Employee
NXP Employee

Hello,

  shortly - "imx6_platform_sdk_v1.1.0" is not valid (supported) and

it was not intended for i.MX6UL.
""fsl-gpu-sdk-2.3.bin" - this is just for GPU of i.MX6.

Regards,

Yuri.