Is iMX53 FlexCAN SRX_DIS bit setting fail?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is iMX53 FlexCAN SRX_DIS bit setting fail?

3,053 Views
Ushnek
Contributor I

Dear All,

          I am trying to setup the CAN bus for transmitting and receiving message by socketcan library. (cansend and candump)

     However, the flexcan(can0) always can receive the message frame which send by itself even if I set the register "SRX_DIS" of flexcan to "1".

     Would someone help me to set this up please?

Labels (2)
0 Kudos
Reply
7 Replies

2,614 Views
jimmychan
NXP TechSupport
NXP TechSupport

Which BSP are you using?  and apply all the patches?

For your information, here is the link of BSP and patches for i.MX53.

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX53_SW

0 Kudos
Reply

2,614 Views
Ushnek
Contributor I

Hi Jimmy,

     I use the QSB BSP and modify its config for CAN bus transciveing based on mx53_loco and mx53_ard.

     The CAN port could send and receive message with another CAN device. (by cantest tool)

     However, it receive the message sent by itself, too. This is not normal behavior in CAN spec.

     I have added all of the patches for iMX53 when I built image, especially patch about CAN bus.

     Thank you and your response.

0 Kudos
Reply

2,614 Views
ioseph_martinez
NXP Employee
NXP Employee

Hi,

Can you please explain how/when are you setting the srx_dis is being set?

Can you try read with memtool the FLEXCANx_MCR register? check if the SRX_DIS bit is really being set or not.

I am wondering if the feature is really implemented.(if the driver ever sets the bit)

Or if the bit is set during initialization. (It must be set during init, otherwise it may fail)

0 Kudos
Reply

2,614 Views
Ushnek
Contributor I

Hello,

I observed the value of srx_dis by flexcan driver (in the path /sys/devices/platform/FlexCAN.0/)

and the value 1 before and after the driver up.

0 Kudos
Reply

2,614 Views
YixingKong
Senior Contributor IV

Ushnek, please click Correct Answer/Helpful Answer if Ioseph Martinez answered your questions.

Thanks,

Yixing

0 Kudos
Reply

2,614 Views
ioseph_martinez
NXP Employee
NXP Employee

Hi,

Did you try using /unit_tests/memtool?

if you are accessing driver /sys/devices/platform/FlexCAN.0/ I am not sure you are seeing the real srx_dis... but simply a mirrored value or variable of the driver.

With the memtool you will see the exact value on the CAN peripheral register. From ref manual addresses are

FLEXCAN-1_MCR is 53FC_8000h base + 0h offset = 53FC_8000h

FLEXCAN-2_MCR is 53FC_C000h base + 0h offset = 53FC_C000h

Please then check the actual register value and let me know.

0 Kudos
Reply

2,614 Views
Ushnek
Contributor I

Hi all,

          I had used memtool to read register but it would print below message.

     Reading 0x1 count starting at adUnhandled fault: external abort on non-linefetch (0x1018) at 0x2aac5000

     dress 0x53FC8000

     Bus error

     So I am not sure these address could be read by memtool. Maybe these address are not in the trustzone with MMU?

    


          By the way, I find the solution for my flexcan driver issue. According the documentation of socketcan "can.txt"      point this description in section 3.2 and 6.2, I add the device flag "IFF_ECHO" in flexcan/drv.c. The echo message      would not be received itself and srx_dis register could be workable, too. I don't know why flexcan source code is       not add this flag in default.


          After all, the srx_dis bit is workable in my board but the flexcan driver need add IFF_ECHO flag to stop receiving     message sent itself.


Ushnek

    

    

0 Kudos
Reply