Is gpio command supported in uboot for i.mx6 ultralite? (yocto)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Is gpio command supported in uboot for i.mx6 ultralite? (yocto)

1,927 次查看
nathanholder
Contributor I

Is gpio command supported in uboot for i.mx6 ultralite?

I'm working with a DIGI board that does not have gpio command in uboot, at least not enabled, also i am not sure it has the i.mx6 gpio driver.

So if nxp stream has gpio command then I can request they (DIGI) update their yocto stream.

标签 (3)
标记 (3)
0 项奖励
回复
1 回复

1,254 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Nathan

one can look at definition CONFIG_CMD_GPIO in uboot/configs/mx6ul_14x14_evk_defconfig
howoever I am not afraid if it was tested. Also may be helpful
U-Boot programming: A tutorial -- Part II | xillybus.com 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复