Hi Community!
I have a question about the I/O installed in i.MX93.
Is USART(not UART) supported on i.MX93?(Something with serial clock input/output like the one installed in i.MXRT600)
I checked IMX93RM.pdf. Looking at "Figure 1.Simplified Block Diagram", it looks like a total of 8 UARTs/USARTs are installed. But "Chapter 62 Low Power Universal Asynchronous Receiver/Transmitter (LPUART)" does not seem to have any description of USART.
Or is it written in another chapter?
Similarly, IMX93CEC.pdf did not have USART listed.
Best Regards,
KASHIWAGI Takashi
解決済! 解決策の投稿を見る。
Does that mean that "Figure 1.Simplified Block Diagram" in IMX93RM.pdf and the block diagram in product page are a typo?
-->Yes,i think so as there is no such function description in RM.
Best Regards
Zhiming
Please refer Chapter 62 Low Power Universal Asynchronous Receiver/Transmitter (LPUART), no USART support.
Hi @Zhiming_Liu - san
Thank you for reply.
> Please refer Chapter 62 Low Power Universal Asynchronous Receiver/Transmitter (LPUART), no USART support.
I see. Does that mean that "Figure 1.Simplified Block Diagram" in IMX93RM.pdf and the block diagram in product page are a typo?
The block diagram is written as if the i.MX93 is equipped with a USART module.
Best Regards.
KASHIWAGI Takashi.
Does that mean that "Figure 1.Simplified Block Diagram" in IMX93RM.pdf and the block diagram in product page are a typo?
-->Yes,i think so as there is no such function description in RM.
Best Regards
Zhiming
Hi @Zhiming_Liu - san
Thank you for reply!
> Yes,i think so as there is no such function description in RM.
I understand.
Best Regards
KASHIWAGI Takashi