Is TDM Audio configuration only available for SAI1 in i.MX8mq processors?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is TDM Audio configuration only available for SAI1 in i.MX8mq processors?

1,482件の閲覧回数
gabrielrivas
Contributor I

Just a simple question according to the i.MX8mq to confirm the information from the manual, for example if I need to share a SAI bus between 2 or more CODEC ICs, in a TDM configuration, the only way to do this is by using the SAI1?

Thanks

0 件の賞賛
返信
2 返答(返信)

1,466件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Gabriel,

There is PCM in below section 3.5

https://www.nxp.com/docs/en/application-note/AN12202.pdf

And it's also mentioned in below community

https://community.nxp.com/thread/524538

Regards

 

0 件の賞賛
返信

1,448件の閲覧回数
gabrielrivas
Contributor I

Hi, thanks for your response. I had a look at the documentation you make reference and I had seen some responses on the support forums like : https://community.nxp.com/t5/i-MX-Processors/How-to-setup-sai1-tdm-mode-for-imx8mq-evk/m-p/888020

In the documentation they mention that in order to transfer several channels ( not clear if data or audio channels) you need to configure the bit fields TCE[] or RCE[] for Tx or Rx respectively. In the i.mx8 reference manual section 13.10 it says that this bit fields have to be set, but seems like only for the SAI1 it allows multiple channels, for any other SAI module it only allows 1 channel. I think I need more clarification on how to setup all the registers for TDM.

0 件の賞賛
返信