Is SPL still not supported in uboot-imx?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is SPL still not supported in uboot-imx?

ソリューションへジャンプ
2,518件の閲覧回数
noorahmadshinwa
Contributor III

Hi!

I am trying to build u-boot with HAB support for a custom board, and I am very confused. I would appreciate any support anyone could provide here.

I keep reading on other questions on this forum how the (official) nxp uboot-imx does not support SPL. I cloned what i think is the nxp uboot-imx from here:

git://source.codeaurora.org/external/imx/uboot-imx.git

branch=lf-5.4.y_v2019.04

When I look at the files for mx6sabresd, it sure looks like this version does support and build SPL by default.

Did the official nxp uboot-imx start supporting SPL or did i clone the wrong repo?

Thank you.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,452件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Noorahmadshinwari

latest nxp uboot releases from source.codeaurora.org/external/imx/uboot-imx support spl.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,453件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Noorahmadshinwari

latest nxp uboot releases from source.codeaurora.org/external/imx/uboot-imx support spl.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,452件の閲覧回数
noorahmadshinwa
Contributor III

Hi Igor,

Thank you for your response.

I would appreciate it if you could have a look at my related question here:

https://community.nxp.com/message/1346580 

Thanks again!

0 件の賞賛
返信