Hello Community,
I've built U-boot.bin file for a customized board, taking sabreauto U-boot as reference.
Now i would like to copy U-boot binary to external RAM using MfG tool.
1). Is It required to configure MFG tool specific configuration in Board config files(.h & .c) to copy U-Boot binary alone?
(as far as i know, it is only required when we need to copy kernel along with u-boot).
I'm getting error when i try to load to eRAM, attached Mfg tool log. When i connect JTAG to see updated DCD values,
they are set to default values, not able to see updated values from imximage.cfg input file.
checked also in U-boot.bin file with editor tool, there is no mention about DCD registers, why so?
Please help, Thanks.
Original Attachment has been moved to: MfgTool.log.zip
Hello,
You are right : it is not needed to change U-boot sources in order to
load U-boot binary image to memory. Looks like the i.MX6 in Your case
is not in serial (USB) boot mode.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Yuri,
I have USB OTG(HID mode) to download U-boot.bin to eRAM and a serial port to see booting log in Console.
I suspect RAM is not initialized by DCD values(DCD is provided by hardware expert, so there may not be a problem with calibrated values).
However I would like to cross check DCD information in U-boot.bin once, Is there a way?
Thanks.
Hello,
1.
Please check if it is possible to load and run (NXP) U-boot on NXP board via
MFG.
2.
RAM may be not initialized in secure boot, since IVT, DCD must be signed in such case.
Regards,
Yuri.