Is JTAG required to flash images on imx8 custom board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is JTAG required to flash images on imx8 custom board

3,986 Views
shilesh_babu
Contributor II

Dear NXP,

we are developing a custom board based on i.MX 8MQuad application processor, for images flashing on board uuu tool or mfg tool is enough jtag is not needed.

as per my understanding jtag used only when on board debugging is required.

Tags (1)
6 Replies

3,889 Views
igorpadykov
NXP Employee
NXP Employee

Hi Shilesh

you are right jtag is not needed for  flashing images, it is

used for debugging.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,889 Views
shilesh_babu
Contributor II

Thank you for your help igorpadykov, As i am planning to use i.MX 8M Nano custom board, could you please suggest me which are JTAGs are good to debug i.MX 8M Nano custom board. 

0 Kudos
Reply

3,889 Views
igorpadykov
NXP Employee
NXP Employee
0 Kudos
Reply

3,889 Views
shilesh_babu
Contributor II

thanks for your quick response, 

Is Segger J-Link doesn't support IMX8m.Nano ?
0 Kudos
Reply

3,889 Views
shilesh_babu
Contributor II

Hello igorpadykov‌,

As SEGGER is not supporting IMX8m.Nano  for debugging now could you please suggest other one.

thanks.

0 Kudos
Reply

3,889 Views
igorpadykov
NXP Employee
NXP Employee

one can consider Lauterbach tools

Best regards
igor

0 Kudos
Reply