Is GPU/IPU libs for Gst 1.x supported on imx_4.1.15_2.0.0_ga?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is GPU/IPU libs for Gst 1.x supported on imx_4.1.15_2.0.0_ga?

729 Views
wenmingfeng
Contributor III

Hi 

recently a new kernel release imx_4.1.15_2.0.0_ga is on git of freescale. Does this kernel support also including the GPU/IPU graphics accelarate libs for Gst 1.x?

Anybody used this version and verified the 3D/2D graphics capabilities?

Thanks!

Wenming

Labels (3)
0 Kudos
2 Replies

585 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Wenming,

The BSP release 4.1.15_2.0.0 includes:

- GA release for i.MX 6ULL, i.MX 6Quad/Dual/Plus/Solo/SoloX/SoloLite/Ultralite and i.MX 7Dual 
- Upgrade U-Boot to 2016.03 
- Upgrade Gstreamer to 1.8.1 and multimedia upgrade to 4.1.4 
- Upgrade to Krogoth Yocto Project release with GCC 5.3 
- Kernel and BSP library fixes

and yes it support 3D/2D driver GPU acceleration.

regards

0 Kudos

585 Views
wenmingfeng
Contributor III

Thanks for reply. 

How can I get the configuration file. I am using the buildroot?

Is there a prebuild image with Qt or ubuntu destop?

Regards!

Wenming

0 Kudos