Is GPU/IPU libs for Gst 1.x supported on imx_4.1.15_2.0.0_ga?
03-14-2017
07:22 AM
1,023 次查看
wenmingfeng
Contributor III
Hi
recently a new kernel release imx_4.1.15_2.0.0_ga is on git of freescale. Does this kernel support also including the GPU/IPU graphics accelarate libs for Gst 1.x?
Anybody used this version and verified the 3D/2D graphics capabilities?
Thanks!
Wenming
2 回复数
03-14-2017
11:16 AM
879 次查看
Bio_TICFSL
NXP TechSupport
Hi Wenming,
The BSP release 4.1.15_2.0.0 includes:
- GA release for i.MX 6ULL, i.MX 6Quad/Dual/Plus/Solo/SoloX/SoloLite/Ultralite and i.MX 7Dual
- Upgrade U-Boot to 2016.03
- Upgrade Gstreamer to 1.8.1 and multimedia upgrade to 4.1.4
- Upgrade to Krogoth Yocto Project release with GCC 5.3
- Kernel and BSP library fixes
and yes it support 3D/2D driver GPU acceleration.
regards
03-15-2017
06:33 AM
879 次查看
wenmingfeng
Contributor III
Thanks for reply.
How can I get the configuration file. I am using the buildroot?
Is there a prebuild image with Qt or ubuntu destop?
Regards!
Wenming