Is 8/9/16/18-bit 6800-series/8080-series parallel Interface available on i.MX6?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is 8/9/16/18-bit 6800-series/8080-series parallel Interface available on i.MX6?

Jump to solution
1,279 Views
shree97
Contributor II

Hello all,

While reading the Display data sheet I came to know that it can be interface using 8/9/16/18-bit 6800-series/8080-series Parallel Interface.

But I didn't find any reference to this interface in the i.MX6 documentation.

So, I just want to know whether this interface is available on the i.MX6 ?

Best Regards,

SR

Tags (1)
0 Kudos
1 Solution
1,014 Views
igorpadykov
NXP Employee
NXP Employee

Hi shree97

asynchronous displays (smart lcds) are not supported by IPU of i.MX6DQ/SDL processors.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

3 Replies
1,014 Views
shree97
Contributor II

Is it possible to implement this System-80 interface using GPIO pins?

If yes, kindly guide me for it.

Thanks & Regards,

SR

0 Kudos
1,015 Views
igorpadykov
NXP Employee
NXP Employee

Hi shree97

asynchronous displays (smart lcds) are not supported by IPU of i.MX6DQ/SDL processors.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,014 Views
shree97
Contributor II

Thanks igorpadykov for your reply.

0 Kudos