Interrupts on iMX35 board with 2.6.38 kernel

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Interrupts on iMX35 board with 2.6.38 kernel

528 Views
JeffCunningham
Contributor I

Greetings.

I am working with an iMX35 board (an RPC353) trying to get to work with a 2.6.38 kernel patched for ARM support. The kernel is built and works fine with the board. The remaining issue is enabling the gpio for interrupt handling in our module which previously worked with a .31 kernel. 

What I am hoping to find are one or two examples of code for a similar board which use the new functions and interface. In particular

rpc_gpio_input

set_irq_type

request_irq

free_irq

Much obliged,

Jeff Cunningham

Tags (1)
0 Kudos
Reply
0 Replies