Dear All,
Hello. I have questions about Interruption frequency of SDMA & SSI.
Please check and answer for attached file.
Best Regards,
Keita
解決済! 解決策の投稿を見る。
In aplay
https://fossies.org/dox/alsa-utils-1.1.0/aplay_8c_source.html
parameter "--buffer-size", finally defining the counter,
may be setup from command line.
~Yuri.
Hello,
Basically Your understanding is correct ; but usually interrupts of
CPU are caused after total operation is completed. Each burst of data
transfer is not needed to be served. Generally it is required to setup
source, destination addresses and number of bytes to transfer.
Transfer consists of several bursts, depending on FIFO size. When
transfer completed, CPU interrupt is asserted. Please refer to bit I (19)
of Bufffer descriptor in Table 55-49 (Buffer Descriptor Field Descriptions)
of the i.MX6 D/Q RM : “When SDMA has finished to process data transfer
attached to this buffer descriptor, send an interrupt to the ARM platform.”
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Yuri,
Thank you for your information!
> Generally it is required to setup
> source, destination addresses and number of bytes to transfer.
We found the count setting of Buffer descriptor was 768 Bytes in jb4.2.2_1.1.0.
So, in case of "Fs = 44.1kHz & Transfer bit = 16bit x 2ch = 32bit";
(768Byte/4Byte) * (1/44.1kHz) = 4.35ms
And, I measured the Interruption frequency was 4.35ms on custom board, too.
Next, in case of "Fs = 96kHz & Transfer bit = 24bit x 2ch = 48bit"
(768Byte/6Byte) * (1/96kHz) = 1.33ms
The interruption frequency was very high!
[Questions]
[Q1]
Is my above calculating equation right?
[Q2]
Could you tell me the way to increase the count of BufferDescriptor to decrease the interruption frequency?
And, is there an bad effect by increasing the count?
[Note]
"Setting point of SDMA BD(BufferDescriptor)"
- Source code : drivers\dma\imx-sdma.c
- Function : static struct dma_async_tx_descriptor *sdma_prep_dma_cyclic
"How to measure the "
Insert the "printk" in below code.
- Source code : drivers\dma\imx-sdma.c
- Function :sdma_handle_channel_loop
Best Regards,
Keita
Hi,
1.
Yes - Your approach is correct.
2.
Table A-1 (SDMA Scripts Overview) of i.MX6 D/Q RM states
about SSI mcu_2_ssiapp script, where thre is counter parameter from
"Parameters Through Buffer Descriptor" column. This is the number
of bytes to transmit. You may try to play with it.
Regards,
Yuri.
Hi Yuri,
Thank you for your reply.
> 2.
> Table A-1 (SDMA Scripts Overview) of i.MX6 D/Q RM states
> about SSI mcu_2_ssiapp script, where thre is counter parameter from
> "Parameters Through Buffer Descriptor" column. This is the number
> of bytes to transmit. You may try to play with it.
Sorry for my poor understanding.
Could you tell me the detail steps to change the counter parameter?
3.
Is there an bad effect by increasing the count parameter?
Best Regards,
Keita
Hello,
what is BSP release ?
Regards,
Yuri.
Hi Yuri,
Sorry.
My customer is using jb4.2.2_1.1.0.
Best Regards,
Keita
Hello,
really, number of bytes to transfer is provided by an application.
Regards,
Yuri.
Hi Yuri,
> really, number of bytes to transfer is provided by an application.
No.
My question was below.
Could you tell me how to set (change) the counter parameter to decrease the interruption frequency?
Best Regards,
Keita
Keita, hi !
Android jb4.2.2 is based on Linux 3.0.35 kernel.
Kernel driver setups burst length ; buffer addresses and total length
to transfer is provided by an application.
Regards,
Yuri.
Dear Yuri,
Hello.
I understood that to increase Buffer descriptor (Current 768 Bytes), it is necessary to set from Application.
Do you have an sample application to test setting the counter parameter?
(It is OK the sample app on Linux. ex. Unit test or gstreamer...)
Best Regards,
Keita
In aplay
https://fossies.org/dox/alsa-utils-1.1.0/aplay_8c_source.html
parameter "--buffer-size", finally defining the counter,
may be setup from command line.
~Yuri.