Interrupt geneartion between Cortex-A53 & Cortex-M4 in imx8mm

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Interrupt geneartion between Cortex-A53 & Cortex-M4 in imx8mm

556 Views
prasannakulkarni
Contributor IV

I too have similar question!!, what is the purpose of keeping M4 along with Cortex -A53 in imx8mmini or so? What are the best examples

which have been already implemented using these cores ?

I was going though Reference manual of imx8m Message Unit Section, explains about so many concepts, but are there any examples to verify those? I want to send an interrupt from M4 to A53 or vice versa by making use of below concepts. I could find very few examples in mcuexpress sdk that too simple messaging examples.... is OpenAmp supported on imx8m platform? or only RPmsglite works?

 

4.3.2.7.1 Interrupts to the Processors
There are 12 interrupt sources from the MU to the Processors:
• Four receive interrupts (asserted when the Processors receive full bits are set and
enabled in the xCR register) for each of the receive registers
• Four transmit interrupts (asserted when the Processor transmit empty bits are set and
enabled in the xCR register) for each of the transmit registers
• Four general purpose interrupts (asserted when the GIP bits are set and enabled in the
xCR register)

 

kindly update

0 Kudos
Reply
1 Reply

509 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

 

 

 

The Linux side will call imx_rproc_xtr_mbox_init->mbox_request_channel_byname->mbox_request_channel->imx_mu_dcfg to realize RX/TX message, but the mailbox driver miss the code for Generic interrupt, you can refer this case : https://community.nxp.com/t5/i-MX-Processors/imx8mm-Wake-Linux-from-M4-core/m-p/1492800

0 Kudos
Reply