Internet on IMX6 quad core with pre-loaded android image

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Internet on IMX6 quad core with pre-loaded android image

864件の閲覧回数
danielromero
Contributor I

I cannot get the internet to work on an IMX6 quad core demo board. Is there wifi on the board? I am also plugged into the ethernet port. Is this supported on the pre-loaded android image? Thanks.

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

727件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Daniel Romero,

It does support the ethernet. About wifi you need to confirm if there is wifi module in the board.
Have a great day,
Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信