Internal MAC clock frequency for Ehernet of i.MX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Internal MAC clock frequency for Ehernet of i.MX6

Jump to solution
792 Views
yuuki
Senior Contributor II

Dear All,

I want to set frequency of MII clock(MDC pin).

I refer to the following point.

IMX6DQRM.pdf (Rev2)
- 23.5.7 MII Speed Control Register (ENET_MSCR) (P.1100)
- Table 23-12. Programming Examples for MSCR (P.1100)

Internal MAC clock frequency is listed in Table 23-12.
However, I do not know which this frequency shows.

Is this frequency set in DIV_SELECT Field of CCM_ANALOG_PLL_ENETn registers?

May I have advice?

Best Regards,
Yuuki

Labels (1)
0 Kudos
1 Solution
573 Views
igorpadykov
NXP Employee
NXP Employee

Hi yuuki

yes correct, internal MAC clock frequency is

set in DIV_SELECT Field of CCM_ANALOG_PLL_ENETn register.

Best regards

chip
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
574 Views
igorpadykov
NXP Employee
NXP Employee

Hi yuuki

yes correct, internal MAC clock frequency is

set in DIV_SELECT Field of CCM_ANALOG_PLL_ENETn register.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos