Internal MAC clock frequency for Ehernet of i.MX6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Internal MAC clock frequency for Ehernet of i.MX6

跳至解决方案
1,465 次查看
yuuki
Senior Contributor II

Dear All,

I want to set frequency of MII clock(MDC pin).

I refer to the following point.

IMX6DQRM.pdf (Rev2)
- 23.5.7 MII Speed Control Register (ENET_MSCR) (P.1100)
- Table 23-12. Programming Examples for MSCR (P.1100)

Internal MAC clock frequency is listed in Table 23-12.
However, I do not know which this frequency shows.

Is this frequency set in DIV_SELECT Field of CCM_ANALOG_PLL_ENETn registers?

May I have advice?

Best Regards,
Yuuki

标签 (1)
0 项奖励
回复
1 解答
1,246 次查看
igorpadykov
NXP Employee
NXP Employee

Hi yuuki

yes correct, internal MAC clock frequency is

set in DIV_SELECT Field of CCM_ANALOG_PLL_ENETn register.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,247 次查看
igorpadykov
NXP Employee
NXP Employee

Hi yuuki

yes correct, internal MAC clock frequency is

set in DIV_SELECT Field of CCM_ANALOG_PLL_ENETn register.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复