Interlaced video output from HDMI on i.mx 8m EVK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Interlaced video output from HDMI on i.mx 8m EVK

Jump to solution
988 Views
idi
Contributor I

Hi, I would like to confirm if my understanding is correct or not.

At 15.3.2.5 DTG Interlaced Video Timing Generator in MX8MDQLQRM,
"The DTG supports interlaced timing generation.".

Is this mean EVK can output 1920x1080 59.94i signal from HDMI?

Because there is no "Interlaced signal timing table" on 15.3.2.7 DTG Timing Standards.

And there is an topic about Interlaced video output at https://community.nxp.com/thread/477269.
The answer is "The i.MX8 do not support interlace."

So, I am confusing which is the correct.
1. i.mx8m EVK have capability to output 1920x1080 59.94i from HDMI, but sample software does not support this mode.
2. i.mx8m does not support 1920x1080 59.94i from HDMI. The explanation of 15.3.2.5 is not about interlaced video output from HDMI.

Please help.

1 Solution
793 Views
igorpadykov
NXP Employee
NXP Employee

Hi Y

as stated in sect.13.4.1 Overview i.MX8MDQ Reference Manual

The protocols supported by the controller are: ..• CEA-861-F..
https://www.nxp.com/docs/en/reference-manual/IMX8MDQLQRM.pdf

Extended Display Identification Data - Wikipedia 

which includes some interlaced formats. However NXP i.MX8M BSPs do not support it.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
794 Views
igorpadykov
NXP Employee
NXP Employee

Hi Y

as stated in sect.13.4.1 Overview i.MX8MDQ Reference Manual

The protocols supported by the controller are: ..• CEA-861-F..
https://www.nxp.com/docs/en/reference-manual/IMX8MDQLQRM.pdf

Extended Display Identification Data - Wikipedia 

which includes some interlaced formats. However NXP i.MX8M BSPs do not support it.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------