Interfacing WM8978 audio codec with imx6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Interfacing WM8978 audio codec with imx6

1,222件の閲覧回数
shammi112
Contributor I

Hi,

Is there any reference document which explain connections between imx6 and WM8978 audio codec.

Regards,

SHAMMI

0 件の賞賛
返信
1 返信

995件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi SHAMMI

this depends which audio interface is used, please check SSI connections

description in AN2628 Programming Audio Applications

http://www.nxp.com/docs/en/application-note/AN2628.pdf 

or for SAI : AN4486

http://www.nxp.com/assets/documents/data/en/application-notes/AN4486.pdf 

ESAI : AN18148

http://www.nxp.com/docs/en/application-note/AN1848.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信