Interfacing Marvell Phy 88E1510 in RGMII with iMX6SoloX

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Interfacing Marvell Phy 88E1510 in RGMII with iMX6SoloX

1,822 Views
mchaplet
Contributor II

Hi,

I try to use the Marvell Ethernet Phy 88E1510 with iMX6SoloX.

The 25MHz Quartz input of the Phy is wired on iMX ENET1_RX_CLK muxed in REF_CLK_25M to generate 25MHz.

All RGMII signals are wired correctly (TX/RX_Data[0:3], RX_EN, .... ) as done on Sabre Ref board.

After a quick fixup in marvell driver to add tx clock delay (similarly to AR8031 fixup), the Ethernet works fine in 10/100 Mbps Half/Full duplex.

But the Gigabit is not working at all.

Does it need an additional configuration / wire ?

On the Sabre design, it seems that an output clock of the AR8031 is re-injected in iMX SoloX as "REF_CLK_IN".

Is it necessary to make Gigabit working ?

What are GPR1 and Anatop enet PLL configurations in this case ?

Thanks for your help,

Martin

Labels (1)
0 Kudos
Reply
1 Reply

898 Views
Yuri
NXP Employee
NXP Employee

Hello,


   Looks like, for RGMII, using external clock is more preferable solution
(as for i.MX6). Please use ENET_REF_CLK for it – as input clock from external
Ethernet PHY. Please use the reference design as an example.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply