Interfacing FPGA SDIO interface with imx6 SD3

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Interfacing FPGA SDIO interface with imx6 SD3

1,351 次查看
shammi112
Contributor I

Hello,

We are  trying to interface FPGA using sdio interface on imx6 sd3 interface. But imx6 is not able to detect FPGA SLAVE device. we are getting the below errors.

43.136538] mmc1: queuing unknown CIS tuple 0x01 (0 bytes)
[ 56.955815] mmc1: error -22 whilst initialising SDIO card
[ 59.026637] mmc1: error -110 whilst initialising SDIO card
[ 61.096092] mmc1: error -110 whilst initialising SDIO card
[ 63.166095] mmc1: error -110 whilst initialising SDIO card

Regards,

SHAMMI

0 项奖励
回复
1 回复

1,126 次查看
art
NXP Employee
NXP Employee

Most likely, it means that your FPGA is not configured properly to be recognized as an SDIO device. Please check your FPGA configuration first.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复