Interfacing FPGA SDIO interface with imx6 SD3

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Interfacing FPGA SDIO interface with imx6 SD3

1,353件の閲覧回数
shammi112
Contributor I

Hello,

We are  trying to interface FPGA using sdio interface on imx6 sd3 interface. But imx6 is not able to detect FPGA SLAVE device. we are getting the below errors.

43.136538] mmc1: queuing unknown CIS tuple 0x01 (0 bytes)
[ 56.955815] mmc1: error -22 whilst initialising SDIO card
[ 59.026637] mmc1: error -110 whilst initialising SDIO card
[ 61.096092] mmc1: error -110 whilst initialising SDIO card
[ 63.166095] mmc1: error -110 whilst initialising SDIO card

Regards,

SHAMMI

0 件の賞賛
返信
1 返信

1,128件の閲覧回数
art
NXP Employee
NXP Employee

Most likely, it means that your FPGA is not configured properly to be recognized as an SDIO device. Please check your FPGA configuration first.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信