Interfacing DDR3 with iMX535

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Interfacing DDR3 with iMX535

Jump to solution
871 Views
sherry_zahid
Contributor III

Link me to the documents for interfacing DDR3 with iMX535. Thanks

Labels (1)
1 Solution
746 Views
igorpadykov
NXP Employee
NXP Employee

Hi Sherry

please check i.MX53 System Development User’s Guide

http://www.freescale.com/files/32bit/doc/user_guide/MX53UG.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

2 Replies
747 Views
igorpadykov
NXP Employee
NXP Employee

Hi Sherry

please check i.MX53 System Development User’s Guide

http://www.freescale.com/files/32bit/doc/user_guide/MX53UG.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

746 Views
sherry_zahid
Contributor III

Thanks for the response Igor,

Where to obtain IBIS models for the iMX535 DDR3 @ 1.5V and 120 Ohm ODT?

What is the difference between IBIS models with ODT vs Driver impedance?

e.g. what does driver impedance refer to? (these are the names of IBIS models for iMX535)

lpddr2hs_sel10_ds001_mio     -    DDR, 1.2V, lpddr2 mode, 240 Ohm driver impedance

ddr2odths_t21_sel00_mi          -     DDR, 1.8V, ddr2 mode, 21 Ohm ODT

Regards,

0 Kudos
Reply